cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX 4.17.0 ,"you are not connected to internet" error is showing

SV
Associate

Hi,

when TouchGFX 4.17.0 is opened I'm getting an error stating no internet connectivity even though my laptop is connected to internet . also in the selection of boards I'm not getting any board option .

thanks and regards

sinduja

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Solved.

Guess the server was just down...

View solution in original post

60 REPLIES 60
bvege.1
Associate

I have the same issue after updating from previous version v4.16.

Thanks,

VBK

DSafa.1
Associate

i also have same problem..

my connection internet no have problem.. no use proxy.. and i think good connection..

already instal and uninstal.. even redownload the software on website.. but still same..

try instal version 4.17.0 and 4.16.1 same problem..0693W00000D0Xi3QAF.jpganyone can help.. pls.

Thanks

Deni

QLiu.4
Associate

me too...0693W00000D0XqCQAV.png

GMont.3
Associate

I have the same issue, version 4.17 " You are not connected to internet and no demo or examples are available.

Anyway, the application is great! Thanks.

VAgga
Associate II

Hi,

I am also facing the same issue with all versions of TouchGFX.  " You are not connected to internet and no demo or examples are available

IGomesMSc
Associate II

Hi,

I also have same problem...

YGroh.1
Associate

Hi,

I am having the same problems. No Internet connection, no demos, no examples, no boards to select...

Due to other problems I also just set up a completely new Windows system and newly installed all the latest STM Software with default settings. Still doesnt work...

Solved.

Guess the server was just down...

MG32
Associate II

Hi,

I have the same problem with 4.17.0:

"No Internet connection"

Is the server down again?

Or could it be a problem with internet settings?

How can a proxy be configured in TouchGFX designer?

Thanks.