cancel
Showing results for 
Search instead for 
Did you mean: 

Why are the PWM pulses distorted when I set the duty cycle of the pulse cycle 1% -3% and 98% -99%?

Adam_K
Associate II

Hi, I configured PWM 25 kHz on Nucleo-767ZI to control the PWM fan.

When I set up Duty Cycle 1% -3% and 98% -99% the PWM signal is deformed.

When the Duty Cycle is 4% to 97% PWM signal is good.

Can it be improved or is it normal?

Regards

2 REPLIES 2

That's your oscilloscope's inability to trigger on short pulses, or maybe it's set so (search for "HF rejection, noise rejection" in Trigger settings).

JW

RMcCa
Senior II

This is normal for pwm. Designers often use 5%-95%.​