cancel
Showing results for 
Search instead for 
Did you mean: 

How to use flash loader demonstrator to program STM32F427VI

As.51
Associate III

Hi all,

I have the STM32F427VI connected using serial RS232 cable.

I downlaoded the latest version of the Flash Loader and the parameters are Even/115200/Disabled/8

I tried using jumper on boot 0, boot 1 and boot 0&1 but I can't connect to the MCU.

Any idea what is the problem?

I always get the same error: No response from target

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

Are you resetting the device after pulling BOOT0 high? Those pins are only checked once after reset.

If you feel a post has answered your question, please click "Accept as Solution".

Not much to work with here.

No idea about anything else on the board, or connectivity.

The system should not see signals/noise on other loader related pins described in AN2606.

So no GPS sending data at startup, for instance.

The connection is a one-shot deal, reset try immediately, reset to try again.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
As.51
Associate III

I solved this by putting the pins as you suggested. Thanks