cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with adding a Library to the Projekt.

kcrh73
Associate

I can add the Library over the Properties of Project. Under the c/C++ General topic, Paths and Symbols. With the Tab Libraries.

There i can Add it with the Button Files System.

But if i Build it, i get following Error Message.

How can i solve it?

cannot find lC:/Users/ckregel/STM32CubeIDE/workspace_1.0.1/SPI_Basis/SPI_Basis/Src/libargus.a

collect2.exe: error: ld returned 1 exit status

make: *** [makefile:41: SPI_Basis.elf] Error 1

0 REPLIES 0