cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK V1 recognizes BlueNRG, ST-LINK V2, AND V3 do not

EHill.19
Associate II

The STM32 ST-LINK V1 connects and recognizes the BlueNRG (see STLINK-V1)

for the ST-LINK V2 and V3, the STM32 ST-LINK Utility connects but does recognize the device. same for the STMCubeIDE debug connection

13:38:57 : ST-LINK SN : 56FF6D067878545241190967

13:38:57 : V2J33S7

13:38:57 : Connected via SWD.

13:38:57 : SWD Frequency = 4,0 MHz.

13:38:57 : Connection mode : Normal.

13:38:57 : Debug in Low Power mode enabled.

13:38:57 : Device ID:0xA7F 

13:38:57 : Device family :Unknown device

I have attached the circuit between the SPBTLE-1S and the connector

1 REPLY 1
EHill.19
Associate II

turns out Keil uvision works. but I have to pay $1600

should have stuck with arduino