Skip to main content
DHes
Associate II
July 22, 2019
Question

Problem with using external crystal oscillator

  • July 22, 2019
  • 7 replies
  • 2150 views

Hi Everyone,

We are using the following code to generate clock pulse for STM32F722 from an external 12MHz crystal. However, whatever we do it sounds the STM32F722 gets its clock pulse from an internal 16 MHz oscillator. The reason for using an external 12MHz crystal is because we want to increase the clock pulse frequency up to 120 MHz or higher. I need to mention that there is no hardware problem with the board that we are using. So any help or recommendation for solving this problem will be highly appreciated, thanks.

Here is the code that we are using for generating clock pulse from an external 12MHz crystal:

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_HSE;

 RCC_OscInitStruct.HSEState = RCC_HSE_ON;

 RCC_OscInitStruct.LSIState = RCC_LSI_ON;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

 RCC_OscInitStruct.PLL.PLLM = 6;

 RCC_OscInitStruct.PLL.PLLN = 140;

 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;

 RCC_OscInitStruct.PLL.PLLQ = 3;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

  Error_Handler();

 }

This topic has been closed for replies.

7 replies

Tesla DeLorean
Guru
July 22, 2019

Make sure you clear the RCC_OscInitStruct variable when defining it as a local/auto variable.

Is HAL_RCC_OscConfig() returning an error?

Inspect what the system says it is doing after calling the setup

  printf("Core=%d\n", SystemCoreClock);

  printf("APB1=%d\n", HAL_RCC_GetPCLK1Freq());

  printf("APB2=%d\n", HAL_RCC_GetPCLK2Freq());

Make sure HSE_VALUE is correctly defined.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DHes
DHesAuthor
Associate II
July 22, 2019

Thanks Clive. I really appreciate for your response with information.

Dan

DHes
DHesAuthor
Associate II
August 6, 2019

Hi Clive,

We managed to increase the clock speed for STM32F722 using PLL. Now we are wondering how we can keep the baud rate of USART6 to 115200 bit/s (is there any function/capability in STM32F722 that automatically adjusts the USART clock divider and set the baud rate after changing the Micro's clock speed?)

Your quick response is highly appreciated.

Thanks,

Dan

Tesla DeLorean
Guru
August 6, 2019

Sending USART_Init() again should reconfigure it using current decomposition of clock settings.

https://community.st.com/s/question/0D50X0000BB1OvJSQV/setting-the-usart-baudrate

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
August 6, 2019

For I2C, but relevant

 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_PeriphCLKInitTypeDef RCC_PeriphCLKInitStruct = {0};
 
 /*##-1- Enable the HSI clock #*/
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct)!= HAL_OK)
 {
 /* Error */
 Error_Handler();
 }
 
 /*##-2- Configure HSI as I2C clock source #*/
 RCC_PeriphCLKInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2C1;
 RCC_PeriphCLKInitStruct.I2c1ClockSelection = RCC_I2C1CLKSOURCE_HSI;
 
 HAL_RCCEx_PeriphCLKConfig(&RCC_PeriphCLKInitStruct); 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
August 6, 2019

Somebody (probably @Tilen MAJERLE​ ) was too quick to close the other thread https://community.st.com/s/question/0D50X0000BB1OvJSQV/setting-the-usart-baudrate so I comment here: it's nice that USARTs have the option to choose a different clock in RCC of the 'F722, but IMO HSI is not a great option for USART, especially if the other party uses a similar unprecise RC clock, or if there are other external environmental influences (level conversion, long cables), and/or if the application is expected to be subject to wide operation temperature or supply voltage range and does not implement some form of fine-tuning HSI on the go (if such is possible in 'F722 at all).

OTOH, as Clive said, it's dead easy to adjust the baudrate - switch off UART, rewrite BRR, switch it on again. You may want to wait with the switch until transmitter is empty, otherwise transmitted byte gets garbled. Reception may be affected if characters are arriving while changing clocks, but upper-level protocols should take care of both these problems.

One more related option is autobauding, but I doubt you want to go that way.

JW