cancel
Showing results for 
Search instead for 
Did you mean: 

Stand alone St-link V2 + STM32f4 Discovery Board

officialkesh
Associate III
Posted on July 07, 2015 at 19:43

Hello ,

Stand - alone st-link is not able to detect target IC .....

How can I flash STM32F4 Discovery board chip through stand-alone St-link V2 ?

I have removed both jumpers of CN3 .

I have made following connections with 20 pin JTAG header

(1)   VCC         -  VCC

(7)   SWDIO    -  PA13

(9)   SWCLK   -  PA14

(20) GND        -  GND

(15) NRST      -   NRST 

4 REPLIES 4
Posted on July 07, 2015 at 20:28

Make sure you can measure a supply voltage at the board.

Break the solder-bridge on the NRST

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
nesrine
Senior
Posted on July 08, 2015 at 11:30

Hello,

I reproduce your case with my Discovery board and I have any problem,

1) I remove the 2 jumpers from CN3

2) I connect application to the CN2 debug connector as follow:

1

à

 VDD

2

à

 PA14

3

à

 GND

4

à

PA13

5

à

NRST

I hope this is helpful for you

Syrine

officialkesh
Associate III
Posted on July 08, 2015 at 16:19

Thank you syrine but I do not want to debug/program external controller ....

officialkesh
Associate III
Posted on July 08, 2015 at 16:19

thank you clive1 ..