cancel
Showing results for 
Search instead for 
Did you mean: 

I2C Issues in STM32F215

thirukannan
Associate II
Posted on June 26, 2014 at 12:50

Hi,

I am using STM32F215(master) in my custom board. In this controller is connected to the MPU9150 sensor(slave) via I2C interface.I tried to read the  slave Id of the slave device, but i am getting  whatever i am sending the slave address.Here i note down one thing, after configured the i2c always i am getting the BUSY in SR2 register. I don't know the problem, please help me asap.

Below is my configuration,read and write code for I2C.

static void I2C_Config(void)

{

    GPIO_InitTypeDef  GPIO_InitStructure;

    I2C_InitTypeDef I2C_InitStructure;

     RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);

    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);

 

 

 

  /* GPIO Configuration */

  /*Configure I2C SCL pin */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;

  GPIO_InitStructure.GPIO_PuPd  = GPIO_PuPd_UP;

  GPIO_Init(GPIOB, &GPIO_InitStructure);

 

  /*Configure I2C SDA pin */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;

  GPIO_Init(GPIOB, &GPIO_InitStructure);

    

  /* Connect PXx to I2C_SCL */

 // GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_I2C1);

 

  /* Connect PXx to I2C_SDA */

 // GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_I2C1);

 

   I2C_DeInit(I2C1);

 

  /*!< I2C Struct Initialize */

  I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;

  I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2;

  I2C_InitStructure.I2C_OwnAddress1 = 0xA0;

  I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;

  I2C_InitStructure.I2C_ClockSpeed = I2C_SPEED;

  I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

  I2C_Init(I2C1, &I2C_InitStructure);

  I2C_Cmd(I2C1, ENABLE);

 // I2C_GenerateSTART(I2C1, ENABLE);

}

void MPU_Write(unsigned char Address,unsigned char DataVal)

{

    I2C_GenerateSTART(I2C1, ENABLE);

    I2C_SendData(I2C1,MPU6050_SLAVE_WRT);

    I2C_SendData(I2C1,Address);

    I2C_SendData(I2C1,DataVal);

    I2C_GenerateSTOP(I2C1, ENABLE);

}

unsigned char MPU_Read(unsigned char Address)

{

    int i;

    unsigned char c;

    I2C_GenerateSTART(I2C1, ENABLE);

    I2C_Send7bitAddress(I2C1, 0x68,I2C_Direction_Transmitter);

    I2C_SendData(I2C1,Address);

    I2C_Send7bitAddress(I2C1, 0x68,I2C_Direction_Receiver);

    //for(i=0;i<100000000;i++);

    c=I2C_ReceiveData(I2C1);

    I2C_GenerateSTOP(I2C1, ENABLE);

    return c;

}

Advance thanks for your help.

Regards,

Thirukkannan.P

0 REPLIES 0