cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 - Multi channel PWM input

fakhfakh
Associate
Posted on October 23, 2014 at 01:59

Hello 

I'm using an STM32F405 based board (OpenPilot ) and i'm looking to capture 5 input PWM signals over only two Timers . For this , i have to use multiple channels of the two timers . I succeeded doing it with only one channel using the example provided with the standard library . But i could'nt adapt it to a multi channel case . 

Can someone explain to me how to configure the Timers and how to compute the different dutycyles . An example with more than one channel would help a lot . Thanks.

#pwm-duty-cycle-computation
1 REPLY 1
Gigi
Senior
Posted on December 12, 2014 at 11:16

Ciao

The question is not strictly related to motor control firmware so I suggest to ask it in the general discussion forum regarding STM32 like :

Microcontroller->STM32 Software Tools and Firmware

Ciao

Gigi