cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407VG 6 PWM

yazctaner
Associate
Posted on September 19, 2016 at 23:48

Hi Dear All,

I wanna ask you some questions about 3 phase motor control. If I wanna generate 6 PWM, I have to use both of two Timer? (because of Timer1 and T?mer8 has 4 channels.) And I wanna generate 6 PWM in order to drive 3 phase motor. Each 2 PWM (high side and low side) must be complementary and also deadtime is needed. How can I achive this? It would be appreciated somebody give me advice/guide on this subject?

Thank you very much.

Best Regards.

#stm32-pwm #timer-complementary-dead-time #3phase-motor
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
peterpeter9162
Associate II
Posted on October 03, 2016 at 17:40

You can use any advanced timer with 4ch.  Only need to use one timer because you can use CH1, CH1N, CH2, CH2N, CH3, CH3N outputs.  The CHxN outputs are inverted from the regular channels and you can add deadtime to avoid shoot through.

Chris