cancel
Showing results for 
Search instead for 
Did you mean: 

How to make BIOS default config

cdvehicle
Associate II
Posted on July 26, 2005 at 22:54

How to make BIOS default config

4 REPLIES 4
cdvehicle
Associate II
Posted on July 05, 2005 at 03:01

Default the BIOS startup at a splashscreen , it hide the start information such as memory test,PCI device table. I can close

splash screen in BIOS setup, But It is not convenience. How can I

make the default bios config like AMI's config tool?

kaouther
Associate II
Posted on July 05, 2005 at 05:41

Are you using an evaluation board? If yes, you should have a jumper to clear the CMOS.

You have also the possibility to reset the setting from the splashscreen in the bios setup.

cdvehicle
Associate II
Posted on July 09, 2005 at 14:31

Yes, I use the evlboard. I clear the BIOS setup and resetup it. , such as disable spalsh, change Boot disk.....

But ofter few days , when I open the power, the BIOS has changed to default setup. I check the battary, the voltage is OK.3.2V. Why? Perhaps the BIOS is a evalBIOS, so it has some limited?

marios
Associate II
Posted on July 26, 2005 at 22:54

If I recall correctly, there is a BIOS menu item that documents what are the different features in the demo BIOS from the regular one. Some timed features.

On the 4.3 version of the BIOS I remember that the board was going in halt mode after a while, with a message sayind ''demo timeout'', preventing the installation of any large operating system.