cancel
Showing results for 
Search instead for 
Did you mean: 

Atollic is less than xxxxRed

dthedens2
Associate II
Posted on October 01, 2010 at 21:38

Atollic is less than xxxxRed

#crippleware
2 REPLIES 2
Andrew Neil
Evangelist II
Posted on May 17, 2011 at 14:09

Isn't Atollic the one where the free version is crippled so that you can't use printf?

I don't mean that it just doesn't come with a ready-to-run printf, so that you have to make your own - I mean specifically crippled so that it is impossible for you to add your own...

Andrew Neil
Evangelist II
Posted on May 17, 2011 at 14:09

Yes, it is:

''It is common to redirect the I/O from these functions to the actual embedded platform, such as redirecting printf() output to an LCD display or a serial cable ... The freeLite version of TrueSTUDIO do (sic) not support I/O redirection, and instead have do-nothing stubs compiled into the C runtime library.''

See:

http://www.atollic.com/index.php/kb/1-kb_building/4-kb_redirect_io

See also :

https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/DispForm.aspx?ID=12672