cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX: Restore Default button on peripheral config dialog

John Craven
Senior
Posted on September 23, 2017 at 00:54

I was using the I2C Configuration dialog today, and i messed things up, so i hit the Restore Default button at the bottom of the I2C peripheral properties dialog. 

When i regenerated my project, it compiled with errors, because all my pin User Labels reset too!!!!

Even ones that had nothing to do with I2C, like buttons and LEDs, etc....

I am using v4.22.1. This is a bug!!!

The button on a peripheral config dialog should only reset the peripheral.

Its debatable if it should reset, the associated pins that have been given user labels.

It definitely should not reset other stuff, without a warning!

#cube #restore-default
2 REPLIES 2
Jeanne Joly
Senior III
Posted on February 06, 2018 at 15:15

Hi

Craven.John

,

Sorry for my late reply.

I see your point. We will keep you informed as soon as we have some updates on this topic.

BR. Jeanne

John Craven
Senior
Posted on February 07, 2018 at 15:50

LOL! glad to see you are on it!