cancel
Showing results for 
Search instead for 
Did you mean: 

CRC32 MPEG2 configuration for ST32C0x1 CRC driver

STDoom
Associate II

Hi

I'm trying to understand how to configure the hal/peripheral to evaluate the CRC32 MPEG2 over a block of datas.

I'm comparing the result with this site where as input I've used the vector 0x01, 0x01. Expected result is 0xD66FB816

https://crccalc.com/?crc=0x01,0x01&method=crc32&datatype=hex&outtype=0 

 

I've configured the hal in the following way

hcrc.Instance = CRC;

hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_DISABLE;

hcrc.Init.GeneratingPolynomial = 0x04C11DB7;

hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_DISABLE;

hcrc.Init.InitValue = 0xFFFFFFFF;

hcrc.Init.CRCLength=CRC_POLYLENGTH_32B;

hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;

hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;

hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;

 

NOTE that poly and init value that I've set are equal to the default values

 

but I get this result

0xeec8fd24

 

Does someone has an idea how to configure this peripheral to get the expected result?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

0xeec8fd24 is from pattern { 0x01,0x00,0x00,0x00,0x01,0x00,0x00,0x00 };

Look at how you'd feeding data into the CRC peripheral. What function are you using to pass data?

Feed bytes via *((volatile uint8_t *)&CRC->DR) = byte;

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

0xeec8fd24 is from pattern { 0x01,0x00,0x00,0x00,0x01,0x00,0x00,0x00 };

Look at how you'd feeding data into the CRC peripheral. What function are you using to pass data?

Feed bytes via *((volatile uint8_t *)&CRC->DR) = byte;

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi Tesla

Perfect! I've found the issue.