cancel
Showing results for 
Search instead for 
Did you mean: 

rs485 communication between stm32f103 and a pc

sak hos
Associate III
Posted on June 18, 2017 at 20:04

Hello,

i'm using stm32f103c8t6 in order to send data to my PC using RS485 (max485) and an USB/RS485 adapter , i made the right connection between components and i used uart to send the data to the max485 and i tried to check the data at reception using a hyperterminal and i found that i'm not receiving the correct data.

is there some special configuation to do to uart in order to communication with the max485 (data length , stop bit ...)

thank you 

#rs485
3 REPLIES 3
LMI2
Lead
Posted on June 18, 2017 at 20:19

What I know the RS485 is just a quite simple level shifter. What are you trying to send, Ints or Floats or bytes. Then there is the full duplex and half duplex. Have you terminated the receiving end.

I have just spent some 'quality time' with RS485 connection, and it works. But you must connect it correctly. Have your PC and controller a common ground. Maxim probably has application notes and such for RS485 and Max485.

Edit: Do you know that you can connect your MAX chip for local echo. That is RX+ to TX+ and so on. At least it worked with my chip and helped knowing where the trouble was (in wiring).

Posted on June 18, 2017 at 21:02

The settings would need to be coherent.

Send a stream of 'U' characters, review the signalling on the scope, verify the bit timings,etc.

Make sure the HSE, HSE_VALUE, and PLL setting are correct, and that you can verify the clocks with a scope.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on June 18, 2017 at 20:33

i declared as information to send a uint8_t with a value 0x22 or 0xBB

i'm using half dubplex and i putted DE and RE to High level (to use max485 as transmitter ) i added a picture of my RS485/USB adaptaer, it's small circuit wich use a MAX485 and CH340G

thank you for the reply0690X00000603t8QAA.jpg