Resolved! H563ZI I3C SETDASA
Hello! How can i send a SETDASA to bus with my H563ZI as controller? Thanks for help!
Hello! How can i send a SETDASA to bus with my H563ZI as controller? Thanks for help!
I'm new to STM and I'm trying to use USART to communicate between MCU board and my computer. I'm now using USART2 and CP2102 to translate TTL to USB. And have succeeded. But my goal is to directly use USB-C of STLINK to output serial data, because th...
Hi allI am looking for a solution to prevent the NULCEO-H563ZI board from resetting every time the USB-C cable to the PC is plugged in and out. The virtual COM port of the ST-LINK is used to send configuration data to the board. Therefore, it is not ...
Hello,I am trying to develop an external loader application for the STM32H563ZI which is connected to a QSPI flash of type W25Q129JV. I have managed to create a project as described in the ST example. My problem is that the call to HAL_RCC_ClockConfi...
Hello ! Ijust found my h563zit6 has an 8-bytes rxfifo in i3c. I attach it to another i3c controller , and it olny received 8 bytes data. How can i receive data larger than 8 bytes? Thanks!
Hello, I think there's a bug in CubeIDE when working with a Nucleo-H563ZI. Steps to reproduce it:- create new project, clear pinouts- enable USART3 in async mode, PB10 and PC4 pins are assigned (why not PD8 and PD9? don't understand)- ctrl+click on P...
I have a H563ZIT6 . I attach its I3C(used as target) to an I3C controller, and then i find that there is no register for static address in target mode in I3C of H563ZIT6, i just find DEVR0 for dynamic address. Does I3C of H563ZIT6 support static addr...
Hi All,Can anyone share me the STM32H563VG reference schematics or schematics of EVAL board for the same
Hi, I'm planning to buy STM32H503 board and X-NUCLEO-IKS01A3 to study I3C protocol. Before I buy those, I'm making sure I can program the code for I3C to compile it. and found the document on below link.https://www.st.com/resource/en/application_note...
currently I'm trying to understand how to generate and build the project with STM32H503RBI just followed the below link but there is no stm32h5xx_util_i3c.h in "inc/" folder https://wiki.st.com/stm32mcu/wiki/Getting_started_with_I3C I can't also find...