User Activity

Hello,I found an "edge" case with TouchGFX Designer.I have a message box that can swap syntax between language and wildcard count.think of:-ID1: "Clock stop"-ID2: "Clock <min>"-ID3: "Clock <sec>.<usec>"I was able to set a base class with id3 and both...
Hello,I am trying to add warnings to widget when an error happens (shake / judder).I first started looking at the MoveAnimator class but there is no way to "ease" if the startXY == endXY.Other than hand rolling the position myself (as Gaetan shows), ...
1) Using the definition I found here (Wolfram-Stadium).Would it be possible to add an option in the flex button to change into a flex-Stadium/button?I ask this because I saw multiple implementation of keyboards and most of them instantiate way to man...
Kudos from
Kudos given to