User Activity

Hi!I've since given up on utilizing VL53L1X for liquid level measurement. @John E KVAM had previously reccomended me to use instead the VL53L4CD sensor for this sort of application (small recipients with water), and I plan to ship it next week. But I...
Hello again!I've been trying to measure water level using the VL53L1 sensor and reading forum posts on it, and I've gathered that RefSPAD calibration isn't really recommended anymore.From my research on the topic, I know that water reflects only 2% o...
Hi!I have two short questions regarding the dynamic SPAD selection happening on the VL53L1 sensor discussed previously here:- Is there a minimum number of SPADs after the selection? As in, by utilizing a 4x4 region, should I expect no oscillations (t...
Hello.I’m utilizing the VL53L1 sensor to measure water level inside of a closed water bucket.While using a 30cm tall white bucket half full, with the VL53L1 positioned at the top aiming down at the air-water interface, the sensor sometimes outputs in...
Kudos from
Kudos given to