2024-10-18 05:49 AM
Hi!
I have two short questions regarding the dynamic SPAD selection happening on the VL53L1 sensor discussed previously here:
- Is there a minimum number of SPADs after the selection? As in, by utilizing a 4x4 region, should I expect no oscillations (the ones I showed on the other post) due to the selection?
- Is there a direct way to find which specific SPADs are being used after the selection? So I could use it to troubleshoot if the weird distance measurements were caused by it or other factors I didn't take into account.
Thanks in advance!