User Activity

I have a question regarding voltage level I/O compatibility for STM32 MCUs. The sensors providing analog output within a 0–5V range, while those with digital output at either 0V or 12V. Although some GPIO pins on the MCU are 5V tolerant, they are sca...
Hi EveryoneI am currently researching about the STM32H7S78-DK development kit and am exploring its graphics interface capabilities. I would like to know if STM or any other source provides reference code, example projects, or application notes demons...
Hi!I have a custom STM32H753ZIT6 MCU based board for which I am using SWD in order to bootload/program the MCU. To interface the SWD to either the STLINK or other programming modules similar to it, does anyone have any recommendation on what connect ...
If I have a bare h753 MCU on my custom board. What connection in terms of communication peripherals and connectors do I need to achieve. Basically, I want to bootload the MCU. The next step is to be able to program, monitor, test simultaneously. From...
I have the main MCU serving as the master in the spi communication whose primary job is to transmit data over SPI lines to two slaves. If I choose hardware NSS signal configuration the IOC file assigns a default pin as the NSS signal for that SPIx pe...
Kudos given to