cancel
Showing results for 
Search instead for 
Did you mean: 

Optimizing 12V GPIO Logic Level Conversion: 5V vs. 3.3V on STM32H753ZIT6

hvs_learn
Associate III

I have a 12V GPIO high logic input on my board. Should I convert it to a 5V logic level or a 3.3V logic level? Previously, I have implemented 12V to 5V logic level conversion and already have components for this conversion in my inventory. If feasible, can I proceed with 12V to 5V conversion, or is it generally more advantageous to convert 12V high to 3.3V logic level for better compatibility or performance? Is there any recommended project/schematic/component that I should look into for this application?

1 ACCEPTED SOLUTION

Accepted Solutions
gbm
Principal

For most use cases, 2 resistor divider is enough (like 27k + 10k). For some, even one serial resistor is enough.

Any details?

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

View solution in original post

3 REPLIES 3
gbm
Principal

For most use cases, 2 resistor divider is enough (like 27k + 10k). For some, even one serial resistor is enough.

Any details?

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
hvs_learn
Associate III

I want to know if the pins are 5V tolerant or just 3V3 tolerant?

See in ds of your cpu. pin list...

 

But anyway: this is a 3v3 cpu, so use 3v3 level for input signals. Not a difficult decision .

If you feel a post has answered your question, please click "Accept as Solution".