User Activity

Hi,St Community!I tried to use the RFAL library that provides support for ST25TV commands such as PresentPasword and WritePassword.However, it is still not possible to set a password for the user memory area on the card.My specific operation process ...
Hi!St Community My goal is to set a password for the user memory area on the card.During the process of writing the encryption code for the card, I read the manual for the ST25TV02KC.   Based on the underlined sentence in the image, I first send the ...
At the beginning of the program, I first performed a write-then-read operation on register 00 using I²C timing. I wrote 0x04 to register 00, and this worked correctly. However, when I used the same method to perform a write-then-read operation on reg...
Hi ST CommunityI have a ST25TV tag,The UID is E0 02 08 03 8F 65 C9 F5(8bytes)I use the board of NUCLE0-NFC08A1 and the demo in NFC6 generated by Cube MX.I can read the relevant information of the card through the SPI provided in the demo and  than pr...
Kudos given to