User Activity

Hi, Everyone,I am having a strange problem with my board loaded STM32F103C8T6:Case 1: With blank MCU, Bootloader via USART1 can only be activated ONCE after power up. (Boot0 pin was soldered to Vcc for testing.) It will never be able to enter BL agai...
Hello folks,Does any body know why the input pin can not be driven high enough when it is set as the trigger to TIM3 in OPM? I use CubeMX to generate the init code where TIM3 ch1 as input trigger and ch2 as the output. On the board, I use a comparato...
Posted on July 09, 2015 at 22:13Hi, I am using the discovery board to try OPM on timer 2. I can not get it going with any effort on my code list below. Please help!!! It is important to our new product.void GPIO_Configuration(void);int main(void){  ...
Kudos from