2024-10-27 01:33 AM
Hi ,
In table 32 in the Datasheet we can see TXDRP parameter which describes RF output power drop versus supply voltage.
is there also RF frequency offset as a result of the supply voltage drop ? If the answer is yes - can you estimate it ?
Thank you,
Viola
2024-10-27 10:20 AM
What is yoyr RF frequency source? How large is the frequency chance vs supply voltage.
2024-10-27 11:32 PM
Hi,
My RF Frequency source is 32MHZ TCXO which has +- 0.1 PPM Frequency offset for +-5 percent change of TCXO supply voltage.
But , my question is regarding the Synthesizer inside the STM32WLE5 - Does changing the one of the power supplies for the STM32WLE5 device has influence on the Synthesizer output frequency ?
Thanks,
Viola
2024-10-28 02:03 PM
I am quit sure, the synthesizer in effect is digital and there is no effective drift with voltage beside the drift of the input clock.
2024-10-28 07:53 PM
It is mentioned in the datasheet that there is Auto-calibration of the RF-PLL after transition between certain RF power saving modes or when invoked manually . But i didnt see any additional info regarding that .perhaps that also insures there is no drift in PLL output frequency ?