User Activity

I've been trying to get DMA to work on the STM32H7S3L8 with bare metal code. As far as I can tell, I have everything set up correctly(?). I get no DMA error flags. The DMA complete flag is never set and the target buffer remains empty.I have enabled ...
Hello,I'm trying out both the DMAs on the STM32H7S3L8. I am trying to keep it as simple as possible, so I am not using linked list mode (I think. CxLLR is 0). When using HPDMA, I get a Data Transfer Error when trying to copy from SRAM1 to DTCM. The d...
Hello,I'm trying to use the USB-HS peripheral with the built-in PHY on Nucleo STM32H7S3L8I'm using CubeMX generated code from CubeIDE. I have not chosen the Nucleo board on CubeMX, because it was causing some issues with the MPU. Instead, I've chosen...
Kudos from
Kudos given to