cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32g4 op amp

Repwoc
Associate III

Is there a spice model for these op amps?  I am using a stm32g474ce.

3 REPLIES 3
STTwo-32
ST Employee

Hello @Repwoc 

The CAD Ressources of the STM32G474CE are available on this link. For the Operational amplifier only, there is no CAD Ressources available for any of the MCU internal components.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

AScha.3
Super User

afaik - no.

But you could use standard opamp model just setting its parameters as given in ds ->

AScha3_0-1723365264311.png

The parameters depend on the setting you choose for the opamp.

Then you can simulate with the opamp, as you set it.

If you feel a post has answered your question, please click "Accept as Solution".

OK, thank you.  I will try to figure out how to do that.