Yes, the integrated bootloader maybe does not support the CAN interface. But sure a custom bootloader can use whatever interface is available in the controller to receive a new firmware.I didn't use it yet, but have a look at the OpenBLT bootloader w...
Check the RTC init code of your HAL/LL. I remember that I had to add a check if the RTC is already initialized and running, because the default code always did a re-init the RTC on startup.
Make sure your virtual function is non-blocking. From your description it seems like you have a while-loop or similar checking for the release of the FlexButton. But TouchGFX will freeze when the called function is blocking.
If you have 5 instances of your CustomContainer on your View, you can give every instance a different text:myContainer1.getTextArea.setTypedText(touchgfx::TypedText(T_TEXT1));
myContainer2.getTextArea.setTypedText(touchgfx::TypedText(T_TEXT2));
myCon...
You have to add a public method to your CustomContainer-class, for example void setText(Unicode::Unichar * text);And copy the text to your textfield wildcard array. Then you can call this method from your Main screen view class.Another way could be e...