User Activity

I am using an Ethernet switch with three ports. The first Ethernet port (IP address 192.168.1.206) is connected to a CPU. The second Ethernet port is connected to an STM32H743ZIT6 board, and the third Ethernet port is connected to another STM32H743ZI...
Hello Guys, I'm working in stm32h743 series in ethernet and i use latest version stm32 cube mx and toolchain is stm32 cube ide latest version , many times i tried but now i'm tired . Can anyone please help me with this communication protocol? If anyo...
Hi, I am frequently getting tired while working with the STM32H743ZIT6 144-pin Nucleo board / STM32H743IIT6 controller board and an externally connected Ethernet module using a communication protocol. Despite trying many different ways, it is still n...
Hope all is going well. I'm trying to ping STM32H743ZI NUCLEO 144 using LWIP middle-ware. Code generated by CubeMX. Configurations: Set the HCLK to 400 MHzEnabled the CPU ICache and DCache (under Cortex_M7 Configuration)Enabled MPU (Region0, Region1 ...
Hii I'm currently working stm32h743IITx 176  pins stm32cube mx v 6.2.0 . i used ethernet in lwip middleware are used my currently using firmware version 1.9.1 but couldn't connect udp cilent in ethernet   .  No ping, no nothing. Currently I test with...
Kudos from