2022-01-05 3:14 AM
Hello Experts,
Here am using one slave which has SMBUS interface for data transmitting.
I am using STM32F103RBT6 for SM BUS and generating the code with STM CUBE MX ,but am unable generate the working code with it and its generating error code.
I updated the STM32F1 Patch and Cube Mx also still am unable to generate the code.
Does STM32F1 has SMBUS with HAL libraries?
2022-01-05 6:11 AM
Hello @HRedd.1 ,
There is no Driver SMBus for STM32F1.
Can you please share the exact error with your project, this will help me to check the issue.
Imen
2022-01-05 8:39 PM
thanks for the reply.....
this the code am getting after generation.
static void MX_I2C1_SMBUS_Init(void)
{
/* USER CODE BEGIN I2C1_Init 0 */
/* USER CODE END I2C1_Init 0 */
/* USER CODE BEGIN I2C1_Init 1 */
/* USER CODE END I2C1_Init 1 */
/* USER CODE BEGIN I2C1_Init 2 */
/* USER CODE END I2C1_Init 2 */
}
its not generating the full code..
at present am using cube mx 6.1.1...
Please update me the the version where i can generate full code for SMBUS with STM32F1..
2022-01-05 8:40 PM
When can I expect ST to solve this issue?
2022-01-06 1:32 AM
Hi @HRedd.1 ,
It seems the I2C configuration code under main.c is missed.
Could you please confirm if this issue is reproduced with the latest version of CubeMX (v6.4.0) ?
I'm adding CubeMx expert to the loop to check this issue.
Hi @Khouloud ZEMMELI ,
Can you please review this issue related to CubeMx tool - depends on the ticket ID 100162 -
(PS: ticket ID 100162, this is an internal tracking number and is not accessible or usable by customers)
Thanks
Imen
2022-01-06 4:50 AM
Hello @Imen DAHMEN ,
This issue is not related to CubeMX, it is actually a FW issue, the SMBus driver is not yet available for F1 series.
Could you please report this issue to the FW team ?
Thanks,
Sara.
2022-01-06 4:57 AM
Thanks @Sara BEN HADJ YAHYA,
The issue is already escalated to FW team.
Imen
2024-06-13 12:00 AM
hey can you please confirm if the its 2024 if the support for stm32f103 is been added or not?
2024-06-13 12:22 AM
Yes, the STM32F1 series microcontrollers, including the STM32F103RBT6, do support the SMBus (System Management Bus) interface. However, there are a few things to keep in mind:
HAL Libraries Support: The HAL (Hardware Abstraction Layer) libraries provided by STMicroelectronics include support for SMBus communication protocols. This means you can use HAL functions to configure and communicate over the SMBus interface.
CubeMX Configuration: When using STM32CubeMX to generate code, you need to ensure that you configure the correct peripheral (I2C in this case, since SMBus is based on I2C) and set the appropriate parameters such as clock speed, addressing mode, and other parameters specific to your SMBus communication requirements.
Error Generation: If STM32CubeMX is generating errors when you try to configure the SMBus/I2C peripheral, there could be several reasons:
Update and Compatibility: You mentioned updating STM32F1 patch and CubeMX, which is good practice. Ensure that the updates are correctly applied and that there are no compatibility issues between the selected device and the tool versions.
To troubleshoot the issue further:
If you provide specific error messages or details about the issues you're encountering during code generation, I can help you troubleshoot further.
2024-06-13 6:21 AM
Sadly yes im getting error in the code generation of SMBUS peripheral, can you please help me on this & is there a documentation where we have steps to implement this.