User Activity

Dear Community,I'm working on STM32H743ZIT6 based project.Here I want to set up 4 ADCs which have SPI interface.On developer's forum is said "If all ADCs will be sampled at the same point in time with the same settings, then the SCLK, CS, and SDI can...
Hello Community,According to data sheet of STM32H743VIT6 https://eu.mouser.com/datasheet/2/389/stm32h743vi-1760857.pdf1) Dual mode Quad-SPI memory interface running up to 133 MHz2) NOR/NAND Flash memory clocked up to 100 MHz in Synchronous mode Q1: I...
Hi,I'm looking for SRAM memory for STM32H757xI and found thishttps://eu.mouser.com/ProductDetail/ISSI/IS66WVS4M8BLL-104NLI?qs=doiCPypUmgHfByEUFkOsAw%3D%3DDoes such kind or SRAM memory work with this MCU model?Thanks.
Kudos from