User Activity

Hello,I have an STM32H743 on a custom application PCB and I need to use the IWDG as well as the standby mode to save precious battery current.I have noticed the following strange behavior:1 - I mass erase the STM32H743 using STM32CubeProgrammer2 - I ...
Hello, I have written a Flash bootloader for the STM32H743 for our custom application PCB. In a nutshell, the flash bootloader check an external flash memory IC with SPI on the custom application PCB if there is a new image to be flash and do it if i...
Hello,I am evaluating the STM32H723 with the NUCLEO-H723ZG board and I need to use the standby mode with GPIO wake-up.On the board, I have added a 10k pull-down resistor between pin PA0 (connector CN10 pin 29) and GND. I also have wire that I use to ...
Hello,I'm trying to communicate with the USB FS CDC on my NUCLEO-H723ZG while using FreeRTOS and the device doesn't enumerate properly. I am using the current up-to-date software pack for STM32H7 -> 1.11.2I use the CubeMX starting project with the NU...
Kudos from
Kudos given to