Skip to main content
Associate II
March 26, 2024
Solved

USB PD in STM32L562

  • March 26, 2024
  • 7 replies
  • 1890 views

Hi Team, 

I need to build USB PD program on ST32L562, The voltage they are expecting is up to 45V. How to do this?

Regards

Nithin

This topic has been closed for replies.
Best answer by Peter BENSCH

Welcome @NITHIN, to the community!

USB PD currently defines a maximum voltage of 20V, so the expected 45V cannot currently be achieved with USB PD without detours.

Correction: with the new specification for USBPD PD 3.1, a new voltage range is available in EPR mode (Extended Power Range). In contrast to SPR (Standard Power Range), EPR can now also negotiate 48V at 5A = 240W, provided a suitable USB PD source is available. ST is currently developing the appropriate hardware for sink and source.

Regards
/Peter

7 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
March 26, 2024

Welcome @NITHIN, to the community!

USB PD currently defines a maximum voltage of 20V, so the expected 45V cannot currently be achieved with USB PD without detours.

Correction: with the new specification for USBPD PD 3.1, a new voltage range is available in EPR mode (Extended Power Range). In contrast to SPR (Standard Power Range), EPR can now also negotiate 48V at 5A = 240W, provided a suitable USB PD source is available. ST is currently developing the appropriate hardware for sink and source.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
NITHINAuthor
Associate II
March 26, 2024

Hi Peter,

Can i use a voltage divider ckt or a voltage regulator to achieve this? 

Regards

Nithin

 

Peter BENSCH
ST Technical Moderator
March 26, 2024

No.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
NITHINAuthor
Associate II
April 1, 2024

Hi Peter,

which all boards are available in the market with inbuilt EPD?

Is STM32L562 evaluation kit, a good option?

Regards

NITHIN