User Activity

Hello,I am using a STM32H747i-DISCO kit and have set up a project based on the TouchGFX Designer demo applications, which works based on a single framebuffer.If I go into the CubeMX settings and set the framebuffer strategy to "Double Buffer" and the...
 Hello,I use the STM32H747 running at 400 MHz (M7) together with a display that has a resolution of 800x480 pixels.I have set up a project in TouchGFX Designer based on the Gauge example project.The design includes 2 gauges. The chrome ART is enabled...