Hello @TZiel.1,Unfortunately, there is no PDM example currently available. But we are working on providing such example.Thanks for your contribution.Dor_RH
Hello @TZiel.1,Here are some specific application notes, tutorials, and resources that focus on PDM to PCM conversion and using STM32CubeIDE:AN3998: This application note provides detailed information on how to use digital MEMS microphones with STM32...
Hello @Zaim01,Here are some links from STMicroelectronics that can help you write code to configure and use SPI with DMA on STM32 microcontrollers, as well as specific examples for LCD screens using the ST7565 controller:AN4776 Application Note: This...
Hello @KPort , Yes, TouchGFX uses the tick from the OS to progress through the frames, providing a sense of time passing. The interrupt from LTDC starts the rendering of the next frame, indicating that the display is ready to receive the new frame. H...
Hello @Nowy,To resolve this issue, ensure the board is properly powered and verify the boot configuration settings (BOOT0 and BOOT1 pins). Make sure they are correctly set for USB bootloader mode. Additionally, refer to: STM32CubeProgrammer User M...