cancel
Showing results for 
Search instead for 
Did you mean: 

User USB (CN13) of NUCLEO-F446ZE not recognized when stocking on NUCLEO-IHM07M1

apexyz
Associate II

I encountered a weird problem when configuring user USB (CN13) of NUCLEO-F446ZE as a virtual COM port. If no other board (e.g., NUCLEO-IHM07M1) is stocked on, this USB can be recognized as a COM port in Windows 10. However, once NUCLEO-IHM07M1 is mounted, immediately the following message pops up. Any idea about the reasons? How to fix such an issue? 

apexyz_0-1708313581897.png

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @apexyz, to the community!

Well, if you take a look at the schematics of the NUCLEO (MB1137), you will see that CN13 is the connector for the User USB port and PA9 (USB_VBUS), PA10 (USB_ID), PA11 (USB_DM) and PA12 (USB_DP) are used for this purpose, which are led out at CN12.21, CN12.33, CN12.14 and CN12.12.

If you take another look at the schematics of the X-NUCLEO-IHM07M1 (tab CAD Resources), you will discover that these pins lead via CN10 to the signals IN2, IN3, DIAG/EN and CPOUT.

If you plug an X-NUCLEO into a NUCLEO, you must therefore always check carefully whether the functions required by the X-NUCLEO are still free to use on the NUCLEO.

Hope that answers your question?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @apexyz, to the community!

Well, if you take a look at the schematics of the NUCLEO (MB1137), you will see that CN13 is the connector for the User USB port and PA9 (USB_VBUS), PA10 (USB_ID), PA11 (USB_DM) and PA12 (USB_DP) are used for this purpose, which are led out at CN12.21, CN12.33, CN12.14 and CN12.12.

If you take another look at the schematics of the X-NUCLEO-IHM07M1 (tab CAD Resources), you will discover that these pins lead via CN10 to the signals IN2, IN3, DIAG/EN and CPOUT.

If you plug an X-NUCLEO into a NUCLEO, you must therefore always check carefully whether the functions required by the X-NUCLEO are still free to use on the NUCLEO.

Hope that answers your question?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.