User Activity

Hi everyone,We’re working with the STM32H730 microcontroller and have a test setup for displaying content on a screen using LTDC. The test currently fills a buffer in external RAM, which is configured on internal flash memory. The result is as expect...
 Hello ST Community,I’ve been working on a project to enable TouchGFX on my STM32H735-DK, but instead of using the TouchGFX Designer, I decided to configure everything manually to display a pre-designed image on the screen.The IssueInitially, everyth...
Hi STM32 enthusiasts, I’m reaching out to the community for advice and guidance on an issue we’re facing while developing an external loader for our custom board. We’ve been working with the STM32H730IBK6Q chip and an external memory MX25LM51245GXDI0...
Hello ST Community,I’m working on a project where I initially developed software on the STM32H735 evaluation board. Now, I need to port this project to a custom board using the STM32H730 microcontroller. The external flash memory is the same as the o...
Hi everyone,I’m currently facing an issue related to bootloaders and FreeRTOS on STM32 microcontrollers, specifically the STM32H735 and STM32H730.Here’s the background:STM32H735 Development Board: I have successfully implemented a bootloader that jum...
Kudos from
Kudos given to