User Activity

Hello!I have a home made panel with STM32H753 mcu. First, the program was created with a display with a FT5426 type touch controller, and it works flawlessly.I bought another display with a GT911 controller.I modified a gt911 driver a bit, which was ...
Hi!Why can i not disable the protection? I use W25Q256. I can't write and erase the flash ic.The programming was working, but suddenly an error occurred during download. Here I noticed that the bits of SR 1 went to 1 and I can't reset them.What could...
Hello.I would use a static graph to display data. In the handletickevent function, I update the addDataPoint(x data, y data) function for the given page, but nothing appears on the graph, the scale is fine, but no line or change in the x direction ca...
Hello!  My project is almost finished, but I had a little problem. On the dashboard, I can optionally read the speed and coolanz water temperature from the can bus or with sensors (vr sensor, ntc). In the case of the can bus, the display works proper...
Hi everybody!I implemented a keyboard into my project. (I tested the keyboard widget in a separated project, and it worked well).If I use the keyboard in my dashboard project, it make weird things.If i entry a value, i write to the eeprom(M95320). If...
Kudos from
Kudos given to