User Activity

Hi all,I have a setup where many devices need to to respond to a message on 868MHz from a sender. At the moment I am using random delay to space the responses but I will like to use the RadioIsChannelFree() function.Do anyone use this function? Is it...
Hi All,Happy New Year.I am trying to get two STM32WL55 Nucleo boards communicating with each other on the 868MHz ISM band. The structure is  that one boards sends a message and the other board responds with a reply to the message received from the fi...
Hi @STTwo-32Apologies to anyone that would have seen this topic elsewhere on the ST community forum. I was advice to create a new topic.The first time I reported this bug I thought it was a red herring as I did not know how reproduce the bug at will ...
All,When the SubGHz_Phy_PingPong example for the NUCLEO-WL55JC1 project is built without any modification meaning no change to the SubGHz_Phy_PingPong.ioc file everything is fine. I can build and even program the built code to the NUCLEO-WL55JC1 boar...
Hi all,I have three STM32WL55 boards and I am following the STM32WL_WS Workshop tutorial. I can programmed one of the boards using SubGHz_Phy_Base_Station.bin and build the sensor SubGHz_Phy_PingPong project for the other two boards using the followi...
Kudos from