User Activity

Posted on May 09, 2018 at 00:03Is it possible to stop the regular conversion in continuous scan mode (on STM32F437) and start from the beginning without disabling the ADC (to not affect the injected channels conversion )? I.e. when all required samp...
Posted on May 03, 2018 at 23:59Can someone explain me how USB HS is clocked, when using embedded PHY?
Posted on May 03, 2018 at 22:48I have a problem with STM32F437, USB OTG Library 2.2.0  and USB HS with embedded PHY, CDC device.First enumeration never pass in the right way (see the attached file).After unplugging and plugging the cable, everything...
Posted on March 21, 2018 at 10:37Hi,I have question about maximum modulation index in motor control library. When it is 100% is there any danger at very low RPM high side driver's bootstrap capacitors to be completely discharged? Is there any mechan...
Posted on September 08, 2017 at 21:04Hi,I'm building dual bldc motor driving board, using the ST Motor control library. MCU is STM32F303VC. According the motor control workbench, I can select ADC3/4 plus TIM1 for motor 1 and ADC1/2 plus TIM8 for mot...
Kudos from
Kudos given to