User Activity

HI,Is there any way to reset SFLP "Game vector" readings at runtime, once SFLP enabled?For instance, after few minutes of SFLP run, it reports (after quaternion to Euler conversion) YAW: 1.5, PITCH: 0.5, ROLL: 0.1. And I'd like to reset Yaw to 0 (zer...
Hi, newly released CubeMX 6.11.1 still doesn't fix an issue that ThreadX cannot be selected for TouchGFX for TrustZone-enabled projects. It has been reported and admitted quite a while ago. See here:https://community.st.com/t5/stm32-mcus-touchgfx-and...
Hi,after looking into the library code, this forum, and playing for a while with library itself, I'm afraid I know the answer, - yet I'm still required to ask:does TouchGFX (or may be some current or future-planned variants of it) comply with any saf...
Create IOC file with CubeMX at "Root"Generate code from CubeMX for IAROpen "Root\TouchGFX\NGEN_NTZ.touchgfx" in TouchGFX designer and generate the code.It fails, as it tries to update project in "EWARM\Root" instead of "Root\EWARM", i.e. one level up...
Hi,For TrustZone enabled project (U5), TouchGFX configuration in CubeMX can't recognize enabled THREADX.Any ideas?Two screenshots attached:one for TrustZone enabled project setup and another one for the exact same but Non-TrustZone project.For the fo...
Kudos from