cancel
Showing results for 
Search instead for 
Did you mean: 

Reset SFLP on LSM6DSV16?

bear2023R
Associate III

HI,

Is there any way to reset SFLP "Game vector" readings at runtime, once SFLP enabled?

For instance, after few minutes of SFLP run, it reports (after quaternion to Euler conversion) YAW: 1.5, PITCH: 0.5, ROLL: 0.1. And I'd like to reset Yaw to 0 (zero). Is there any way to do so on chip (manipulating offsets, "soft" algorithm reset etc.)?

Surely it is possible to use external matrix to compensate for the above in software but maybe there is some "undocumented" way to ask SFLP to do the same?

 

Thanks

1 REPLY 1
Federica Bossi
ST Employee

Hi @bear2023R ,

Unfortunately, it is not possible to do this.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.