User Activity

I have got 3 identical boards with STM32u5a5. For improving ADC accuracy I want to calibrate Vref using Vrefint. This is working fine on one board, but on the other two boards Vrefint reads as 0 using the same software. Other ADC channels seem to wor...
Hello, I have a problem with unaligned access, which generates a hard fault when the software is started without bootloader.When running the same software from mcuboot bootloader, there is no hard fault on unaligned access.The MPU and TrustZone confi...
I am trying to use TrustZone on STM32U5A9:I am setting up the following regions in SAU:0xc1fe000-0xc1fffff non-secure callable0x8200000-0x83fffff non-secure0x200c0000-0x20273fff non-secure0x60000000-0x6fffffff non-secureAs soon as I flip the enable f...
I am trying to access a NOR flash via OctoSPI1. CLK is connected to PF4, NCS is connected to PI5. While I can see clock cycles on PF4, PI5 stays high all the time.Does anyone have an idea, what could be wrong?Trust zone is disabled. The register sett...
Kudos from
Kudos given to