User Activity

Hi. I'm trying to use STM32H573IIKxQ's SPI using HAL.I've noticed that the HAL library disables the SPI after each transfer which causes the SCK pin to go high and goes low again before the next transfer, which causes an extra bit being shifted to th...
Hi. Is there any consideration that I need to take care of when I use HAL_GetUIDw0~2 while ICACHE is enabled?even the simplest project with STM32H573IIK3Q that the ICACHE is enabled will get a hardfault when trying to get UID bytes.This is the whole ...
Hi. I'm trying to create a software package using Open CMSIS-pack standard which is documented at https://open-cmsis-pack.github.io/Open-CMSIS-Pack-Spec/main/I want to include multiple components from different sources and I want each component to sh...
I can open, regenerate, build and flash B-U585I-IOT02A -> Ux_Device_HID example successfully. But when I try disable USBPD (we don't have usbpd on our board. just the D+ and D- pins) and regenerate the project, so many many unrelated files are being ...
Hi. I'm looking for a (or a bunch of) stm32cube expansion package(s) to add aws iot and freertos mqtt libs to stm32cube. I've found https://www.st.com/en/embedded-software/x-cube-aws-h5.html and https://www.st.com/en/embedded-software/x-cube-aws.html...
Kudos from
Kudos given to