cancel
Showing results for 
Search instead for 
Did you mean: 

Developer package link broken

obedPH
Associate III

Hello,

 

I am having an issue when I try to download the Developer package in the wiki. I am using this link (https://wiki.st.com/stm32mpu/wiki/STM32MPU_Developer_Package#Installing_the_Starter_Package) in the 5.2 section, there, it redirects me to (https://www.st.com/en/embedded-software/stm32mp1dev.html#get-software). In the last link, when I try to download the file, it downloads the wrong file, since it downloads the SDK instead of the Developer package. Probably there is an error in the API and it gets the wrong file. Does anyone else experiences the same issue?

1 ACCEPTED SOLUTION

Accepted Solutions
Pwxn
ST Employee

Hello @obedPH,

 

When you click on the download link, you should select the MP1/2-DEV-SRC and download the latest.

I tried on my side and I could download the developer package without any issue : en.SOURCES-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06.tar.gz

 

The other link are for software development kit specific for each architecture. 

 

I hope this help you.

 

Regards,

View solution in original post

2 REPLIES 2
Pwxn
ST Employee

Hello @obedPH,

 

When you click on the download link, you should select the MP1/2-DEV-SRC and download the latest.

I tried on my side and I could download the developer package without any issue : en.SOURCES-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06.tar.gz

 

The other link are for software development kit specific for each architecture. 

 

I hope this help you.

 

Regards,

obedPH
Associate III

Hello @Pwxn ,

Yes, it worked now, thank you for the reply,

 

 

Regards