User Activity

Hello,I have an issue when compiling a makefile from a project using an STM32H5 and ThreadX with NetXduo library.this is the error i have:make[1]: arm-none-eabi-gcc: Argument list too long make[1]: *** [Makefile:1119: build/TheBlueBox-v2_AZURE_NS.elf...
hello! I start this post because i have created a new project with CUBEMX 6.12.0 and i am having some issues. When I generate code without THREAD X activated, the generation is completed without any error. However, when I add the thread X option (see...
Hello everybody, I am currently designing a configuration utilizing two drivers to heat a mat, which is a resistor load requiring 24V and 3.3A. This component is commuted at 100 Hz. For this setup, I've employed two different drivers: the first one b...
Hello, we are using the saleale logic 8 to read data transfer between an STM32 MCU and an IC through SPI (ADS8166 ADC).The CLK frequency is 1.5 for the SPI configuration with a prescaler of 2 so at the end we have  CLK of 750 kHz. For some reason SO...
Good morning, everyone!I'm new here at the ST forum, so please forgive me if I make any mistakes.Currently, I'm working on migrating the ST25R3916B library for the X-NUCLEO 08A1 DK from ST to Nordic (specifically, nRF52840).I've already replaced all ...
Kudos given to