cancel
Showing results for 
Search instead for 
Did you mean: 

REQUIRED USB DRIVER FOR USB_OTG_FS CONFIGURATION IN STM32H735VGH???

shaktipg
Associate II

Hi! 

Can you recommend me a suitable usb driver to connect STM32H735VGH in device mode ?

And please suggest me if any additional configuration required to work with.

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @shaktipg and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you take a look at the USB_Device examples for the STM32H735G-DK board as a start for your project. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.