User Activity

I have integrated Micro-ROS into the m4. I have it working such that I am able to publish sensor data and receive it from other nodes. However Micro-ROS takes up a quite a bit of space, 70+ KB. In their documentation it is target at mid tier micro co...
I want to be able to have the Ethernet port on my board be configured as a link local address and be able to receive DHCP. How can I accomplish this?
How do I change the pin for the u-boot-stm32mp programmer mode at boot up?
There seems to be an issue with CubeProgrammer and parsing hex strings that are longer than 8 characters. For example, an offset of 0x05984400 will parse correctly but 0x105984400 will not. It will incorrectly parse as 0x05984400. I am trying to refe...
I want to create my own distro for OpenSTLinux but it seems like the envsetup.sh file is dependent on the distro.conf file being located in the meta-st directory. This is a little hard because I am trying to not modify the meta-st layer but am trying...
Kudos from
Kudos given to