Skip to main content
CButz.1
Associate III
Apr 27, 2022 9:35 AM UTC
Solved

USBX device storage class + filex

I want to make a Filesystem with FileX and use the usbx device storage class to get access to the files. I successfully created a FileX filesystem on ram. I found the examples Ux_Device_MSC, this uses the sd card for the file system.

In ux_device_msc.c i have to implement the Status Read and Write commands comming from usb to acces my filesystem.

/* Format the NOR flash as FAT */
	status = fx_media_format(&sram_disk,
							 fx_stm32_sram_driver, 		// Driver entry
							 (VOID*)LX_SRAM_DRIVER_ID, 	// Device info pointer
							 (UCHAR*)media_memory, // Media buffer pointer
							 sizeof(media_memory), // Media buffer size
							 "SRAM DISK", 		// Volume Name
							 1, // Number of FATs
							 32, // Directory Entries
							 0, // Hidden sectors
							 FX_SRAM_DISK_SIZE/512, 	// Total sectors
							 512, // Sector size
							 8, // Sectors per cluster
							 1, // Heads
							 1); // Sectors per track

Currently im using this for read and write, but windows tells me i have to format it, but it should already be a filesystem and second formatting fails.

UINT STORAGE_Read(VOID *storage, ULONG lun, UCHAR *data_pointer,
 ULONG number_blocks, ULONG lba, ULONG *media_status)
{
 UINT status = 0U;
 
 sram_disk.fx_media_driver_request = FX_DRIVER_READ;
 sram_disk.fx_media_driver_logical_sector = lba;
 sram_disk.fx_media_driver_sectors = number_blocks;
 
 fx_stm32_sram_driver(&sram_disk);
 
 memcpy(data_pointer, sram_disk.fx_media_driver_buffer, number_blocks);
 
 return (status);
}
 
UINT STORAGE_Write(VOID *storage, ULONG lun, UCHAR *data_pointer,
 ULONG number_blocks, ULONG lba, ULONG *media_status)
{
 UINT status = 0U;
 
 sram_disk.fx_media_driver_request = FX_DRIVER_WRITE;
 sram_disk.fx_media_driver_logical_sector = lba;
 sram_disk.fx_media_driver_sectors = number_blocks;
 
 fx_stm32_sram_driver(&sram_disk);
 
 memcpy(sram_disk.fx_media_driver_buffer, data_pointer, number_blocks);
 
 return (status);
}

This topic has been closed for replies.
mohamed.ayed
mohamed.ayedBest answer
ST Employee
May 25, 2022 1:14 PM UTC

Hi @CButz.1​ ,

You can refer to usbx_device_mass_storage sample IAR / STM32CubeIDE wihch show USBX Device Mass Storage with SRAM.

Regards.

1 reply

mohamed.ayed
mohamed.ayedBest answer
ST Employee
May 25, 2022 1:14 PM UTC

Hi @CButz.1​ ,

You can refer to usbx_device_mass_storage sample IAR / STM32CubeIDE wihch show USBX Device Mass Storage with SRAM.

Regards.