cancel
Showing results for 
Search instead for 
Did you mean: 

Using a Nucleo-h723 and would like to, via USB DFU, load my program using the built-in bootloader.

GRoss.5
Associate II

Connections:

D- = PA11

D+ = PA12

and Gnd to Gnd

As well, Boot0 is connected to VDD. I have nothing connected to the UARTS or CAN.

Even with this setup, upon reset, the system runs the code I have downloaded (via ST-Link) rather than the bootloader. I think it may have something to do with the crystall.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
KArum.3
Associate

Hi,

First of all ​Nucleo-h723 build-in bootloader is dedicatedly designed for USART software peripheral. So you can't run the on board bootloader otherwise use USART.

MM..1
Chief III

No first of all read AN2606

Pattern 10

Boot(pin) = 0 and BOOT_ADD0(optionbyte) = 0x1FF0

Boot(pin) = 1 and BOOT_ADD1(optionbyte) = 0x1FF0

Check BOOT_ADD

Uwe Bonnes
Chief

Connect both USB ports. Short CN1 Pin5 to Pin 7. Reset via the black button. If you did not fiddle with the option bits, DFU will appear.