User Activity

Hi,   I at a high level I have designed a program to toggle the user LED on PA5 if a gpio input sees a high signal (shorter than 150ms) on PA0.   The program works well most of the time except in some instances when it will miss an input pulse entire...
This code only works when I'm debugging step by step. Otherwise, it always sends ADEN low again, which should not happen!! (Correct sequence: ADEN goes high then ADRDY goes high and both stay high...) (Note both ADEN and ADRDY are low before line 54 ...
Hi, I am looking into using the LIS3MDL 3-Axis Magnetometer in an application with high frequency oscillating magnetic fields. I have looked through the datasheet of the LIS3MDL and it seems to meet most requirements that I've checked. My application...
Kudos from